Scheduled Action Objects
These Action Objects (AO) are user defined calculations scheduled to execute at defined intervals. The Action Object Manager provides valuable information about these processes.
Header |
Description |
Name |
The name given to the AO, saved in the application creating the blueprint. The default name is the name of the file and the AO will be deployed with this name. If a name clash occurs, names will automatically be made unique. |
Status |
|
Next execute |
The time when the next execution of the scheduled blueprint will begin. |
Last start |
The start time of the last executed AO. |
Last end |
The end time of the last executed AO. |
Period |
The duration of the execution of the AO. |
Executes |
The number of AO executions that have been completed. |
Average |
The average execution time of the AO. |
Total time |
The amount of time lapsed since the first execution of the scheduled AO. |
Related topics: